Add Remote Computer dialog box

How do I open the Add Remote Computer dialog box?
  1. If you are not already in Design mode, click design_mode_button.
  2. In the Asset Catalog, expand the
    FTP and Computer Device Items
    node.
  3. Drag a Remote Computer asset onto the tree in the Asset View.
Use the
Add Remote Computer
dialog box to add a remote computer to the asset tree. You can add a remote computer in the root or in a container.
The device is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the device properties, but leaves the device in the tree.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal