Items in Add Remote Computer dialog box
Items in the dialog box include:
- (Parent)(Read-only) Shows the name of the container into which the generic device is being added.
- Description(Optional) Type a description for the asset. The description will be shown in theArchivetab when the asset is selected. The description can be a maximum of 260 characters.
- NameEnter a unique and meaningful name for the asset. This name will appear in the asset tree. The software defaults toRemote Computer. The name must be unique within the parent container. That is, you can have two devices with the same name in the asset tree, they just can't be in the same container. If you add a device into a container that already has a device of the same name, FactoryTalk AssetCentre will append a number (like_2) to the device name to ensure uniqueness.Asset names can be a maximum of 260 characters. The characters \ / : * ? " < > | are not allowed. The character pair &# is not allowed. A space, tab, underscore (_) or dollar sign ($) cannot be the first character in a name, but can be used elsewhere in the name. The following Microsoft Windows device names cannot be used as asset names, whether upper or lower case, with or without the colon: CON:, PRN:, AUX:, NUL:, COM1:, COM2:, COM3:, COM4:, COM5:, COM6:, COM7:, COM8:, COM9:, LPT1:, LPT2:, LPT3:, LPT4:, LPT5:, LPT6:, LPT7:, LPT8:, and LPT9. For example,Auxiliary Linewould be a valid name whereasAux Linewould not.
- Addressing InfoClick in this field and then click
to specify the network location (UNC path) of this computer, as well as the username and password for access to the computer. - Catalog Information(Optional) Enter the model number of the remote computer.
- Configuration DataClick in this field and then click
to select a binder to use as the configuration data for the asset. This associates the binder with the remote computer asset in FactoryTalk AssetCentre.Be sure to share the folder in the remote computer that will be placed in the binder. The user specified in theAddressing Infofield (above) must have access to the shared folder.TIP:We recommend placing the binder asset within the remote computer in the asset tree. You can accomplish this in a couple ways:- Leave theConfiguration Datafield blank initially when adding the remote computer. Add the binder asset under the remote computer in the asset tree. Then edit the remote computer properties to specify the binder in theConfiguration Datafield.
Add the binder asset anywhere in the asset tree, then add the remote computer asset specifying the binder in theConfiguration Datafield. Drag the binder asset from its initial location to the remote computer asset. - Manufacturer(Optional) Enter the asset's manufacturer.
- Operating System(Optional) Enter the operating system of the remote computer.
- Agent GroupClick in this field and then click
to select the agent group for the remote computer.- When adding the remote computer under the root, the default value of Agent Group isSystem Default.
- When adding the remote computer under a container, the default value of Agent Group isInherit from parent: the parent container’s Agent Group property.
- Asset Number(Optional) Enter an asset number for management or inventory purposes.
- Location(Optional) Enter information about the asset's location in your facility.
- Serial Number(Optional) Enter the asset's serial number.
- Properties Configuration(Optional) This box shows the number of default extended properties configured by theOptions dialog box: Extended Properties. To configure extended properties for the asset, click in this box, and then click
. In the Extended Propertiesdialog box, edit, add, or delete extended properties.
Provide Feedback