Remote I/O PanelView dialog box

How do I open the Remote I/O PanelView dialog box?
  1. Open an Allen-Bradley PanelView device's properties (or add an Allen-Bradley PanelView device to the asset tree).
  2. Click anywhere within the
    Addressing Info
    field and click browse_button_small.
  3. Select the controller to which the PanelView remote I/O device is connected.
  4. Select the
    Remote Input/Output Device
    check box.
  5. Click
    Settings
    .
Use the
Remote I/O PanelView
dialog box to specify the settings for a PanelView connected to an Allen-Bradley PLC-5 or SLC 500 controller via remote I/O.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal