Add Generic Container dialog box
How do I open the Add Generic Container dialog box?
- To enter Design mode if you are not already in it, click
. - In the Asset Catalog, expand theOrganizational Itemsnode.
- Drag a Generic Container onto the tree in the Asset View.
Use the
Add Generic Container
dialog box to add a generic container to the asset tree. You can add a generic container in the root or in another container.Provide Feedback