Export a FactoryTalk View Site Edition backup
Once a backup is created for FactoryTalk View Site Edition, you can export the HMI server information from FactoryTalk AssetCentre Archive.
To export a FactoryTalk View Site Edition backup
- SelectView > Archiveor click theArchivebutton.
- In the asset tree, select a backup file created under FactoryTalk View Site Edition.
- In the lower session of theArchivetab, click theHistorytab.
- Right-click a version in the history list and then selectShow in Application Export Window.
- In theGetdialog box, select the check boxes as needed and then clickOK.TIP:ClickHelpin theGetdialog box for detailed instructions.
- (Optional) If the backup is configured to be encrypted in the asset's properties dialog box, you are prompted to enter the encryption. Enter the encryption and then clickSubmit.
- In theExport FactoryTalk View Site Edition_Backup.apbdialog box, select one or multiple areas you want to export.
- To view and select detailed files included in an HMI server for export, click the browse button in theServer Namecolumn.
- In theName Projectdialog box, whereNameis an HMI server name, select files of an HMI server that you want to export and then clickOK.TIP:ClickHelpin theName Projectdialog box for detailed instructions.
- To export the FactoryTalk Directory data in a BAK file, select theExport FactoryTalk Directory backup filecheck box.
- In theTarget Foldersection, click the browse button to specify a folder to save the exported files.
- ClickExport.
- When a window shows indicating that the operation completes, clickOK.
Provide Feedback