Items in Get dialog box

Items in the dialog box include:
  • Get writable copy
    Retrieve an editable instead of read-only copy of the file or binder. This retrieves the most recent or pinned version into the current working folder.
  • Recursively get files from subfolders
    Place a copy of all files and binders located in subfolders of the selected device, container, or folder into the current working folder. This option is only available when you select a device, container, or folder in the asset tree. It is not available if you select a file or binder.
  • Overwrite checked-out files
    Overwrite any versions of the file or binder in the current working folder with the version you are retrieving from the Archive database.
  • Override local name
    Select this option to provide another name for the file or binder to be placed in the working folder. Select the check box and type a name for the file or binder. When you click
    OK
    , the file or binder is placed in the working folder with the specified name.
  • Override working folders with path
    Select this option to retrieve the file or binder into a temporary working folder, instead of the current working folder (for this Get operation only). Type the exact path of the temporary working folder or click
    Browse
    to select the working folder location where you would like to store the retrieved files.
    To override the working folder, you must have
    Configure Personal Archive Working Folders
    and
    Set Working Folders
    permissions.
  • Comments
    Enter an optional comment to summarize the work. This is helpful when tracking work done to a file or binder. The maximum length for a comment is 2,500 characters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal