Name Project dialog box
How do I open the Name Project dialog box?
- SelectView > Archiveor click theArchivebutton.
- In the asset tree, select a backup file created under FactoryTalk View Site Edition.
- In the lower session of theArchivetab, click theHistorytab.
- Right-click a version in the history list and then selectShow in Application Export Window.
- In theGetdialog box, select the check boxes as needed and then clickOK.TIP:ClickHelpin theGetdialog box for detailed instructions.
- (Optional) If the backup is configured to be encrypted in the asset's properties dialog box, you are prompted to enter the encryption. Enter the encryption and then clickSubmit.
- In theExport FactoryTalk View Site Edition_Backup.apbdialog box, click the browse button in theServer Namecolumn.
In the
Name Project
dialog box, where Name
is an HMI server name, you can select files of an HMI server that you want to export.Point to a file in the tree view to show the tooltip indicating its latest modification time. The structure of the tree view represents the structure of exported folders.
Provide Feedback