Export FactoryTalk View Site Edition_Backup.apb dialog box
How do I open the Export FactoryTalk View Site Edition_Backup.apb dialog box?
- SelectView > Archiveor click theArchivebutton.
- In the asset tree, select a backup file created under FactoryTalk View Site Edition.
- In the lower session of theArchivetab, click theHistorytab.
- Right-click a version in the history list and then selectShow in Application Export Window.
- In theGetdialog box, select the check boxes as needed and then clickOK.TIP:ClickHelpin theGetdialog box for detailed instructions.
- (Optional) If the backup is configured to be encrypted in the asset's properties dialog box, you are prompted to enter the encryption. Enter the encryption and then clickSubmit.
Use the
Export FactoryTalk View Site Edition_Backup.apb
dialog box to:- Select one or multiple areas that you want to export.
- View and select detailed files included in an HMI server for export.
- Choose whether the FactoryTalk Directory data is to be exported.
- Specify the folder where the exported files are saved.
Provide Feedback