Columns in the FactoryTalk View Site Edition_Backup.apb dialog box

The following table describes the columns in the
FactoryTalk View Site Edition_Backup.apb
dialog box.
Columns
Descriptions
Check box
Select a check box in front of a row to include that area in the export. At least one area needs to be selected.
The check box in the first row accelerates the selection of areas in the table. It has the following statuses:
  • FTViewSE Export_none Indicates that no areas are selected.
  • FTViewSE Export_all Indicates that all the areas are selected.
  • FTViewSE Export_partial Indicates that some of the areas are selected.
Area
Shows the areas that include HMI servers. The areas shown here correspond to those created in FactoryTalk View Studio.
Server Type
Shows the server type included in the areas. Currently, only HMI servers can be exported.
Server Name
Shows the name of HMI servers as configured in FactoryTalk View Studio.
Click FTViewSE Export_browse files to view and select files included in the HMI server that you want to export.
Primary Host
Shows the name of the computer that the HMI server is on.
Secondary Host
Shows the name of the computer that is configured as redundancy to HMI server in FactoryTalk View Site Edition.
If it's not configured, the Secondary Host shows
Unavailable
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal