Add files or folders to a binder
Follow the steps to add files or folders to a binder.
To add files or folders to a binder
- Check out the binder.
- Add the files to the working folder on your computer.
- Check the binder back in.
The new files you placed in the working folder are added to the binder if they pass the filter criteria set in the
Binder Properties
dialog box.Provide Feedback