About changing the contents of a binder
The contents of a binder in Archive depend on the files in the working folder and the state of the filters when the binder is checked in. To add files or folders to a binder or remove them from a binder, you need to add files or folders to the working folder or delete them from the working folder.
Provide Feedback