Repair an agent controller's permissions
You can repair permissions for the current account that is running the agent controller. For example, when you install some software such as Siemens S7 Controller (TIA Portal), RA drive, and Logix 5000 before installing the FactoryTalk AssetCentre Agent, you can select
Repair
to make them work correctly.To repair an agent controller's permissions
- Open the FactoryTalk AssetCentre Agent Controller Launch Control Panel.FromWindows Startmenu, selectRockwell Software>FactoryTalk AssetCentre Agent Controller Launch Control Panel.OrNavigate toC:\Program Files (x86)\Rockwell Software\AssetCentre Agents\AgentController, and double-clickRA.FTAC.AgentControllerLaunchPanel.exe.If displayed, clickYeswhen theUser Account Controldialog box prompts for Windows users.
- In theAgent Controller Launch Control Panelwindow, click theRepairbutton.
The agent controller starts repairing the permissions, and permissions for the current identity who is running the agent controller will be repaired.
Provide Feedback