Change the SQL Server user account

It is advisable to leave the SQL Server user account as it was initially set up. There are, however, rare circumstances when you might need to edit the SQL Server user account. (This is the AssetCentreUser account that was set up on the SQL Server during the FactoryTalk AssetCentre server installation.)
To access the Data Source Configuration Wizard, on the FactoryTalk AssetCentre server computer select
Start > Rockwell Software > FactoryTalk Assetcentre Data Source Configuration
. Instructions are provided within the wizard.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal