Add a client computer
Client computers run the FactoryTalk AssetCentre client software, which provides the main interface to FactoryTalk AssetCentre. The client software is the subject of this online help document.
To add a client computer to the FactoryTalk AssetCentre system, simply install the FactoryTalk AssetCentre client software on a computer that meets the system requirements and is connected to the same network as the FactoryTalk AssetCentre server.
To add a client computer
- Install the FactoryTalk AssetCentre client on the computer.Open Internet Explorer on the client computer. In theAddressfield of Internet Explorer, type the following address:http://servername/RockwellSoftware/AssetCentrewhereservernameis the name of your FactoryTalk AssetCentre server.For example, if your FactoryTalk AssetCentre server is called MYSERVER, type:http://MYSERVER/RockwellSoftware/AssetCentreIf you are using SSL, then begin with https:// instead of http://.PressEnter.
- Internet Explorer shows a page from the server that allows you to install the FactoryTalk AssetCentre client software. ClickInstall AssetCentre Client on this computer.
- Once connected to server, follow the on-screen instructions to complete the installation. For detailed instructions, selectHelp > Installation Guideto see theFactoryTalk AssetCentre Installation Guide.
During the installation, the FactoryTalk Services Platform will be installed and the computer will be added to the FactoryTalk Network Directory. If for some reason the client computer is not in the FactoryTalk Network Directory, use the FactoryTalk Administration Console to add it. See the
FactoryTalk Administration Console Help
for instructions on adding a computer.
TIP:
If you have a significant number of computers for which you need to permit or restrict access, consider grouping them in the FactoryTalk Administration Console to make assigning security privileges easier. For example, you can group all computers used in offices away from the plant floor and restrict access to features that should be used only from computers stationed where the user can see the automation system directly.
Provide Feedback