Delete contacts from the Address Book

Follow the steps to permanently remove contacts from all groups and the Address Book.
Prerequisites
  • To delete contacts, you must be granted
    View Address Book
    and
    Edit Address Book
    permissions.
To delete contacts from the Address Book
  1. Select
    View
    >
    Address Book
    .
  2. In the right pane of the Address Book, select the contact to delete.
    TIP:
    To select multiple contacts, use
    Ctrl-Click
    and
    Shift-Click
    .
  3. Click SchedulesDelete.
  4. When prompted to permanently delete the contact, click
    Yes
    (or click
    No
    to leave the contact in the Address Book).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal