View the Address Book
How do I open the Address Book tab?
- SelectView > Address Book.
With the
Address Book
tab, you can:- Create, delete, and modify contact information.
- Sort the Address Book by clicking a column heading. The sort order toggles between descending and ascending order.If you sort a column for which there are no entries (for example, groups do not have email addresses, only the contacts within them do), the blank entries will appear first when the entries are sorted in descending order, and last when the entries are sorted in ascending order.
- Show the contacts by last name by clicking theDisplay by Last Nameoption. Group names appear interspersed in the list of contacts as if the group name was the last name.
- Show the contacts by first name by clicking theDisplay by First Nameoption. Group names are not interspersed in the list of contacts. Rather, groups appear at the top of the contact list when it is in ascending order and at the bottom of the contact list when it is in descending order.
Provide Feedback