Address Book toolbar buttons and their meanings

The following table shows the buttons on the Address Book toolbar and their meanings.
Button
Description
addressbooknew
Add a new contact or group to the Address Book. Added groups appear under the Address Book tree. Added groups and contacts appear in the right pane of the Address Book.
SchedulesDelete
Delete
Remove contacts from just a group, or remove contacts and groups from the entire Address Book. If you remove a group from the Address Book, the group's contacts are not deleted.
addressbookproperties Properties
Modify a contact or group in the Address Book.
addressbookfindbutton
Locate specific contacts or groups in the Address Book to view or modify them.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal