Modify contacts and groups
You can change the properties of a contact or group. For example, if a contact's email address or a contact's name changes, you can modify those properties.
Prerequisites
- To modify contacts and groups, you must be grantedView Address BookandEdit Address Bookpermissions.
To modify contact and group properties
- SelectView>Address Book.
- In the right pane of the Address Book, do one of the following:
- Double-click the contact or group.
- Select the contact or group, and then selectEdit>Properties.
- Click thePropertiesbutton.
- Modify the tab information in theContact namedialog box orGroup namedialog box.
- ClickOK.
Provide Feedback