Create contacts
Add a new contact to the Address Book so that person can receive notifications regarding the progress and outcome of FactoryTalk AssetCentre schedules, tasks, and other system-related events.
Contacts cannot be imported from another email program. More than one user can create contacts simultaneously.
Prerequisites
- To create contacts, you must be grantedView Address BookandEdit Address Bookpermissions.
To create contacts
- Do one of the following to open theNew Contactdialog box:
- SelectView>Address Book, and then click theNewbutton.
- SelectView>Address Book, click the dropdown arrow after theNewbutton, and then selectContact.
- SelectTasks>Add New Address Book Contact.
- Complete the information in theNew Contactdialog box. For the contact to receive notifications, you must enter an email address.TIP:If in your existing email system you have a group with an existing email address (for example, a group of electricians with the email addressAllElectricians@MyCompany.com) to which you want to send notifications through AssetCentre, you can use that existing group's email address. Simply create a contact and give it a name (for example,Electricians) and enter the group's email address (AllElectricians@MyCompany.com) as the contact's default email address. The individual email addresses of the electricians group are not added to the FactoryTalk AssetCentre Address Book.
- ClickOK.
Provide Feedback