New Contact dialog box
How do I open the New Contact dialog box?
Do one of the following to open the
New Contact
dialog box:
- SelectView>Address Book, and then click theNewbutton.
- SelectView>Address Book, click the dropdown arrow after theNewbutton, and then selectContact.
- SelectTasks>Add New Address Book Contact.
Use the
Contact
tab in the New Contact
dialog box to create contacts who can receive notifications regarding the progress and outcome of FactoryTalk AssetCentre schedules, tasks, and other system-related events.Contacts cannot be imported from another email program. More than one user can create contacts simultaneously.
Provide Feedback