Configure the FactoryTalk AssetCentre system to use secure communications (TLS)
FactoryTalk AssetCentre
uses TLS 1.2 for secure communications. We recommend that you disable TLS 1.0 and TLS 1.1 in the system and we strongly recommend that you use a certificate signed by a certificate authority (CA).For more information about TLS protocol version support, see Protocols in TLS/SSL. For more information about the compatible
operating system, see Software requirements in the
FactoryTalk AssetCentre Installation
Guide
.
IMPORTANT:
- When the installation environment is targeted to use TLS 1.3,FactoryTalk AssetCentrerequires both TLS 1.2 and TLS 1.3 to be enabled.FactoryTalk AssetCentrewill not work if only TLS 1.3 is enabled.
- Using the TLS protocol is an essential part for the communication security over your network.
- If you want to configure the protocols as needed, you should use the same protocol for all computers deployed in your network.
For more information about the TLS configuration, see Configure the FactoryTalk AssetCentre
system to use security communications (TLS) in the
FactoryTalk AssetCentre Installation
Guide
.Provide Feedback