Configure a site binding

Before you begin
To configure a site binding
  1. Open the Internet Information Services (IIS) Manager on the
    FactoryTalk AssetCentre
    server computer.
    1. On the taskbar, select ic_search.
    2. In the search box, type
      inetmgr
      , and then press
      Enter
      .
    3. Select the best match result.
      Start page of IIS
  2. Navigate to
    localhost
    >
    Sites
    >
    Default Web Site
    .
    9.0 IG Create site binding_1
  3. Under
    Actions
    , select
    Bindings
    .
    9.0 IG Create site binding_2
  4. In the
    Site Bindings
    dialog, select
    Add
    .
    9.0 IG Create site binding_3
  5. In the
    Add Site Binding
    dialog, configure the following settings.
    9.0 IG Create site binding_4
    For this option...
    Do this...
    Type
    Select
    https
    .
    IP address
    Select
    All Unassigned
    .
    Port
    Keep the default port number 443 or if you needed, you may change it to a self-defined port.
    If you use a self-defined port, you must configure a firewall rule and web services URL.
    Host name
    Type the fully qualified domain name (FQDN) of the
    FactoryTalk AssetCentre
    server.
    SSL certificate
    Select your certificate.
  6. Select
    OK
    .
  7. In the
    Site Bindings
    dialog, the created site binding is listed. Select
    Close
    .
    9.0 IG Create site binding_5
    TIP:
    You can remove the default HTTP site binding and only keep the created HTTPS site binding.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal