Export the created certificate for FactoryTalk AssetCentre server, desktop client, web client, and agent computers

After creating a certificate on the FactoryTalk AssetCentre server computer, export the certificate that will be imported on the FactoryTalk AssetCentre server, desktop client, web client, and agent computers.
To export the created certificate
  1. Open the Internet Information Services (IIS) manager, and then double-click the
    localhost
    node.
  2. In
    Features View
    , double-click
    Server Certificates
    .
    server certificate in IIS
  3. Double-click the certificate that you have created.
  4. Select the
    Details tab
    , and then select
    Copy to File
    .
    detalis of server certificate
  5. On
    Certificate Export Wizard
    , select
    Next
    .
  6. Select
    No, do not export the private key
    , and then select
    Next
    .
    export certificate
  7. Select
    DER encoded binary X.509 (.CER)
    , and then select
    Next
    .
    export certificate
  8. Select
    Browse
    to specify a folder for the certificate, and then select
    Next
    .
  9. Select
    Finish
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal