Equipment View
To access the Equipment View
From the View menu, click
Equipment View
.The
Equipment View
displays a graphical tree view of the application hardware. From the Equipment View
, configure the system type, processor safety time, and battery alarm for each controller. Also define the Status
, Control
, and RTC
variables for controllers. The Equipment View
contains an IO Bus 1 and IO Bus 2 for each Standard or Mixed controller defined in a project. Each IO Bus has 24 slots available for assigning I/O modules. Eurocard controllers only have IO Bus 1, containing 18 slots. The Equipment View
displays the digital and analog I/O modules in their defined slots. From the Equipment View
, enable the HART protocol and HART Pass-Through features for analog I/O modules.
Actions to perform from the
Equipment View
are:- Configure the system type, process safety time, and battery alarm for a controller
- Wire processor variables
- Manually set the real time clock
- Add or edit I/O modules
- Configure I/O modules
- Configure the process safety time for an I/O module
- Wire a status variable to an I/O module
- Wire the channels of an I/O module
- Define threshold values for input modules
- Configure analog I/O channels to support theHART®protocol
- Configure the controller to support theHARTPass-Through feature
To refresh the content in the Equipment View
- Select theEquipment View, then from theViewmenu, clickRefresh.
Provide Feedback