Configuring Processor Variables
The 9110 processor module contains status, control, and RTC variables used by the application. Status variables get data from the processor module while control variables set data in the processor module. RTC variables are used for the real-time clock of the application.
Configure the processor variables from the property page of the controller. Each type of processor variable is wired in a separate tab, as seen in the following:

- Statustab, contains status integers and Booleans supplying data about the controller to the application.
- Controltab, contains control integers and Booleans enabling the application to send data to the controller.
- RTCtab, contains status, program, and control variables for the real time clock. RTC status variables supply the date and time to the application. RTC program variables hold the date and time to be written to the real time clock. RTC control variables set and update the clock.TaskProcedureWire a processor variable
- From the Equipment View, double-click the required controller.The Equipment property page displays.
- From the property page, click one of the following tabs:
- Status
- Control
- RTC
- Each tab displays different processor variables performing specific functions.
- From the processor variable tab, locate the required variable, and in theWirecolumn click
. - The Variable Selector displays.
- From the Variable Selector, select the required variable and clickOK.
Unwire a processor variable- From the Equipment View, double-click the required controller.The Equipment property page displays.
- From the property page, click one of the following tabs:
- Status
- Control
- RTCEach tab displays different processor variables performing specific functions.
- From the processor variable tab, locate the wired variable, and in theUnwirecolumn click
.
Provide Feedback