Status Processor Variables
Status processor variables supply data about the controller to the application. The AADvance controller has these status processor variables:
- Status Integers
- Number of Locked Input Variables
- Number of Locked Output Variables
- Processor Module A Temperature
- Processor Module B Temperature
- Processor Module C Temperature
- Status Booleans
- System Health
- System Health Reset
- Dongle Detected (Voted)
- Processor Module A Online
- Processor Module B Online
- Processor Module C Online
- Processor Module A Health
- Processor Module B Health
- Processor Module C Health
- Processor Module A 24v1 Power Feed Health
- Processor Module B 24v1 Power Feed Health
- Processor Module C 24v1 Power Feed Health
- Processor Module A 24v2 Power Feed Health
- Processor Module B 24v2 Power Feed Health
- Processor Module C 24v2 Power Feed Health
- Processor Module A Ready
- Processor Module B Ready
- Processor Module C Ready
- Processor Module A NVRAM Battery Health
- Processor Module B NVRAM Battery Health
- Processor Module C NVRAM Battery Health
Provide Feedback