Configuring the Controller
From the
Equipment View
, define these properties for controllers: System Type
, Process Safety Time
, Battery Alarm
, and Remote Fault Reset
.
System Type
AADvance controllers support three types of systems: Standard, Eurocard, or Mixed.
System Type | Description |
|---|---|
Standard | IO Bus 1 and 2, each containing 24 slots |
Eurocard | IO Bus 1, containing 18 slots |
Mixed | IO Bus 1 and 2, each containing 24 slots |
The type of system affects the available I/O modules. The
Mixed
controller type enables configuring a standard controller with both Standard
and Eurocard
I/O modules.
TIP:
The required system type must be set before adding I/O
modules to a controller.
Process Safety Time
The process safety time (PST) defines the maximum time in milliseconds that the outputs of a controller remain in the ON state after detecting important diagnostic or application faults. When the defined PST is exceeded, the outputs go into their specified safe states. Set the PST for the controller. The default PST for the controller is 2500 ms. By default, each group of I/O modules inherits the PST from the controller. Also set an alternate PST for each I/O group.
Battery Alarm
The 9110 processor module contains a battery supporting retained variables and the Real Time Clock (RTC) when the system power is turned off. The system contains a processor battery alarm to alert that the battery voltage is low and the battery must be replaced. The battery alarm is enabled by default for
Standard
and Mixed
controllers.
TIP:
The
Battery Alarm
must be disabled for
Eurocard
controllers.Remote Fault Reset
The remote fault reset enables resetting faulty processors in the controller without needing to physically press the
Fault Reset
button located on the T9110 front panel. As well, use the remote fault reset to join processors to a running system. The remote fault reset is required for sub-sea systems since it is impossible to physically manipulate the processors. By default, Remote Fault Reset
is disabled (0x00000000). To enable the feature, a non-zero hexadecimal value must be set matching the combined values of the control integers Allow Remote Fault Reset MSB
and Allow Remote Fault Reset LSB
. Possible values range from 0x00000001 to 0xFFFFFFFF. When enabling Remote Fault Reset
, a warning displays confirming the remote reset of the controller.
TIP:
Set the
System Type
before adding I/O modules.
The defined PST must be larger than the execution time for the application to run. By
default, the battery alarm is enabled. Disable the alarm for sub-sea systems or other
systems lacking a battery. By default, the remote fault reset is disabled. It is recommended
to enable the fault reset for sub-sea systems.To configure the controller system type, process safety time, battery alarm, and remote fault reset
- From theEquipment View, double-click the required controller.TheEquipmentproperty page displays.
- From theEquipmentproperty page, click theProcessortab.
- From theProcessortab, select the requiredSystem Type. Select one of the following:
- Standard
- Eurocard
- MixedTheEquipment Viewrefreshes to display the IO Buses and slots attributed to the specific system type.
- From theProcessortab, in theProcess Safety Timefield, type the required value ranging between 20 ms and 60000 ms.TIP: For large systems, set the PST for the controller to 1500 ms or more, ensuring sufficient time to educate a second or third processor module.
- Set theBattery Alarmvalue toEnabledorDisabled.
- Set theRemote Fault Resetvalue to 0x0 (disabled) or a non-zero hexadecimal value (enabled).
- When enabling the property, a warning displays confirming the action. ClickYesto enableRemote Fault Reset.
Provide Feedback