Configure the Controller I/O
Use the
Equipment View
to add I/O modules to controllers, mimicking the hardware
arrangement of the modules. I/O modules are available in a simplex arrangement or in a
redundant group of two or three modules. When selecting a redundant group, modules are
automatically assigned to the free adjacent slots.
TIP:
In anticipation of modifications to the I/O hardware,
add a duplex/triplex group for a simplex arrangement or a triplex group for a duplex
arrangement. If required, also create a hot swap.
When configuring the controller, select the required system type. Define the system type
before adding any I/O modules. Different I/O modules are available depending on the selected
system type. When the system type is
Mixed
, both Standard and Eurocard I/O modules
are available.Perform the following tasks for I/O modules:
Task | Procedure | ||
Add an I/O module to a controller |
| ||
Move an I/O module to a different slot |
| ||
Remove an I/O module |
|
TIP:
In an I/O module having a duplex or triplex
arrangement, wire the required I/O variables and add them to a dedicated spy list to see
which processor is at fault when a fault occurs.
Provide Feedback