Communication View
To access the Communication View
From the View menu, click
Communication View
.The
Communication View
is a graphical environment that displays aspects of communication information related to communication events. The Communication View
displays a tree-like structure with nodes that expand to show the available communication functions and configurations for the series 9000 equipment.From the
Communication View
, use these protocols with Ethernet networks and serial ports:- Modbus RTU/TCP
- OPC
- SOE
- SNTP
- Serial Tunneling using TCP/IP
- SNCP bindings
- CIP
- Peer-to-Peer
- Quality of Service
In the
Communication View
, select tree nodes to access related communication options for the equipment series. These options display in the property pages. When working in the Communication View
, use the mouse controls or keyboard arrows to navigate. View additional properties for selected elements in the Properties window.
To refresh the Communication View
Refresh the Communication View to display the current version control and debug states.
- Select theCommunication View, then from theViewmenu, clickRefresh.
Provide Feedback