Specifying the Workbench and OPC Communications

For communication with the
OPC®
portal, the
AADvance-Trusted SIS Workstation software®
uses an Ethernet port from those defined for the controller processors. By default, the first configured Ethernet port is selected for communications. Also select different ports. To enable Workbench and OPC communications, map variables for:
  • OPC
  • SOE
To specify the Workbench and OPC communications
  1. In the
    Communication View
    , expand the controller, and double-click
    Workbench & OPC
    .
    The
    Communication
    property page for the Workbench and OPC displays.
  2. In the
    Communication
    property page, select a configured Ethernet port.
    Workbench and OPC use the defined port for communications.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal