Add limits to a variable

Add limits to a variable

Add minimum and maximum limits to numeric variables. Limits impose certain behaviors when the value is outside of the limits.
  1. In
    Project view
    , select the variable.
  2. In
    Properties
    , right-click the numerical variable and select
    New
    Range
    .
  3. Under
    EURange
    , complete:
    • Low limit
      . Enter the low limit for the value of the variable.
    • High limit
      . Enter the upper limit for the value of the variable.
    • Constrain
      . Set to true to constrain the values for the variable for the low and high limits.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal