Create a data grid

Create a data grid

Create a data grid that shows motor properties, including: speed, acceleration, and torque.
  1. Create the data grid:
    1. In
      Project view
      , right-click
      MainWindow (type)
      and select
      New
      Data controls
      Data grid
      .
    2. Hover-over the data grid, select
      Edit
      , and enter
      MotorDataGrid
      .
    3. In
      Properties
      , create a dynamic link between
      Model
      and
      ProjectName
      Model
      MotorObjects
      .
      For more information about dynamic links, see Create dynamic links.
  2. Configure the motor name column:
    1. In
      Properties
      , double-click
      DataGridColumn1
      and enter
      MotorNameCol
    2. Under
      DataItemTemplate
      , create a dynamic link between the
      Text
      property and
      Aliases
      {Item}
      Motor@BrowseName
      TIP: You can select the
      @BrowseName
      attribute by selecting it from the
      Attribute
      drop-down menu at the bottom.
      For more information about dynamic links, see Create dynamic links.
    3. Crete a dynamic link between the
      Order by
      property and
      Aliases
      {Item}
      Motor@BrowseName
      TIP: You can select the
      @BrowseName
      attribute by selecting it from the
      Attribute
      drop-down menu at the bottom.
      For more information about dynamic links, see Create dynamic links.
    4. Set
      Title
      to
      Motor Name
  3. Create the motor speed column:
    1. In
      Properties
      , next to
      Columns
      , select
      Add
      and select
      Text column
      .
    2. Double-click the column name and enter
      MotorSpeedCol
    3. Under
      DataItemTemplate
      , create a dynamic link between
      Text
      and
      Aliases
      {Item}
      Motor
      Speed
      .
      For more information about dynamic links, see Create dynamic links.
    4. Set
      Title
      to
      Speed
  4. Create the motor acceleration column:
    1. In
      Properties
      , next to
      Columns
      , select
      Add
      and select
      Text column
      .
    2. Double-click the column name and enter
      MotorAccelerationCol
    3. Under
      DataItemTemplate
      , create a dynamic link between
      Text
      and
      Aliases
      {Item}
      Motor
      Acceleration
      .
      For more information about dynamic links, see Create dynamic links.
    4. Set
      Title
      to
      Acceleration
  5. Create the motor torque column:
    1. In
      Properties
      , next to
      Columns
      , select
      Add
      and select
      Text column
      .
    2. Double-click the column name and enter
      MotorTorqueCol
    3. Under
      DataItemTemplate
      , create a dynamic link between the
      Text
      property and
      Aliases
      {Item}
      Motor
      Torque
      .
      For more information about dynamic links, see Create dynamic links.
    4. Set the
      Title
      property value to
      Torque
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal