Add graphic objects

Add graphic objects

Add a Switch, Spin box, and LED objects to Page1 of your application.
  1. In
    Project view
    , double-click
    Page1 (type)
    .
    Blank Page1 displays in the editor.
  2. Right-click
    Page1 (type)
    and select
    New
    Base controls
    Switch
    .
  3. Right-click
    Page1 (type)
    and select
    New
    Base controls
    Spin box
    .
  4. Right-click
    Page1 (type)
    and select
    New
    Base controls
    LED
    .
  5. In the editor, arrange the objects according to your preferences.
Arranged graphical objects
(optional) Explore and add more graphic elements. See Object examples and Graphic and layout objects.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal