Create a folder

Create a folder

Create a folder to contain objects in your project.
  1. In
    Project view
    , select the node to contain the folder. Select the project level node to create a folder at the root level.
  2. In the view toolbar, select
    Add
    or right-click the node, and then select
    New
    Folder
    .
The
NewFolder#
appears in
Project view
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal