Debug runtime NetLogic remotely

Debug runtime NetLogic remotely

With Visual Studio, you can remotely debug a runtime NetLogic on Windows systems.
TIP: Remote debugging is not possible on HMIs for security reasons. For more information about remote debugging, see Remote debugging - Visual Studio (Windows) | Microsoft Learn.
To debug NetLogic locally, see Debug NetLogic.
  • On the development machine, download Visual Studio and set as the default code editor. See Set the default code editor.
  • Verify that the client machine and the development machine are connected to the same network.
  1. Configure the remote Windows machine as a target in
    FactoryTalk Optix Studio
    . See Add a deployment target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal