Create a bar graph

Use the bar graph object to display a control’s value at the data source. The bar graph increases or decreases in size to show the changing value. You can configure thresholds for the bar graph to alert the operator to error conditions.
To create a bar graph:
  1. In
    FactoryTalk View Studio
    , in the
    Graphics
    editor, select
    Objects
    >
    Gauge and Graph
    >
    Bar Graph
    . You can also click the bar graph icon in the toolbox.
  2. Drag the mouse to position and draw a rectangle the general size and location you intend the bar graph to be.
  3. In the
    Bar Graph Properties
    dialog box, configure how the bar graph looks, its thresholds, and its tags.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal