Create a bar graph using simple drawing objects

You can use simple drawing objects to create a bar graph.
To create a bar graph for several tags, draw a rectangle for each, defining the animation the same for all objects except for changing the tag each is associated with.
To create a bar graph using simple drawing objects:
  1. In
    FactoryTalk View Studio
    , in the
    Graphics
    editor, select
    Object
    >
    Rectangle
    to draw a rectangle.
  2. Right-click the rectangle and select
    Animation
    >
    Fill
    or
    Height
    to define the animation that uses a tag whose values represent the information you intend to show in the bar graph.
    The rectangle will fill or vary in size to represent the tag's value in relation to its minimum and maximum values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal