How the bar graph works at runtime

The bar graph increases and decreases in size to reflect the value of the
Value
connection at the data source. The bar graph’s behavior at runtime also depends on how you set up thresholds and controls.
Using thresholds
If you set up thresholds for the bar graph, when the value of the Value connection is at or above the threshold value, the color of the fill changes (if you set up different fill colors in the General tab). You can also configure the section of the bar graph at or above the threshold level to blink.
Using controls
If you do not assign the Value connection, the bar graph displays the minimum value.
Opening graphic displays
When you open a display at runtime, the application reads the value of the Value connection and updates the bar graph based on the value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal