Set up a connection for a bar graph
Use the
Connections
tab to set up a connection for a bar graph object.To set up a connection for the bar graph:
- In a display, double-click the object to open theBar Graph Propertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to theValueconnection.
Provide Feedback