Configure general properties of a bar graph
Use the
General
tab of Bar Graph Properties
dialog box to set up general appearance of a bar graph.To set up general properties of a bar graph:
- In theBar Graph Propertiesdialog box, in theGeneraltab, specify the following options if needed:
- Appearance
- Bar graph settings
- Thresholds
Provide Feedback