Set up sample demonstrations
The installation process placed the
SampleDemo1
and SampleDemo2
folders in the BATCHCTL
share on your hard drive. Within each of these SampleDemo
folders are four subfolders that contain the files for the area model. To set up sample demonstrations:
- Add aFactoryTalkSecurity user.
- Configure theFactoryTalk BatchServer to locate the area model.
- Verify the recipes in the area model.
Provide Feedback