Add sample FactoryTalk Security users
For the sample demonstrations file, create
FactoryTalk
user accounts for an operator and an engineer. Create these user accounts in the FactoryTalk
Directory.To add sample
FactoryTalk
Security users:- SelectStart > Rockwell Software >. TheFactoryTalkAdministration ConsoleSelectdialog box opens.FactoryTalkDirectoryIMPORTANT:Administrator privileges are required to perform this procedure.
- SelectNetworkto add this user account to theFactoryTalkNetwork Directory, and selectOK.
- If not already logged on to theFactoryTalkNetwork Directory, theLog On todialog box opens. InFactoryTalkUser name, type the user name for the Administrator that was configured when theFactoryTalkServices Platform was installed.
- InPassword, type the password for the Administrator.
- Verify theDirectoryand selectOK.window opens and displays the specifiedFactoryTalkAdministration ConsoleFactoryTalkDirectory.
- ExpandUsers and Groups.
- Right-click theUsersfolder, and selectNew > Userto create a newFactoryTalkSecurity user account inFactoryTalkDirectory.
- TheNew Userdialog box opens and displays theGeneraltab. In theUser namebox, typeOPER.
- InFull name, typeOperator.
- InPassword, typepassword, and confirm it by re-enteringpasswordin theConfirm Passwordbox.
- SelectCreate.
- Repeat steps 7-11, but this time in theUser Namefield, enterENGand in theFull Namefield, enterEngineer.
- Keep theFactoryTalkAdministration Console open to configure permissions for theseFactoryTalkSecurity users in the next exercise.
Provide Feedback