Configure sample permissions for FactoryTalk Security users
After creating the
FactoryTalk
security users, set up access modes for each FactoryTalk Batch
component to specify which users are permitted to view or perform actions. Configure security settings in the FactoryTalk
Administration Console. To tighten security in the client, remove the All Users
group from the Full Edit
policy setting.To configure sample permissions for
FactoryTalk
Security users:- In theFactoryTalkAdministration Console Explorer pane, navigate toSystem > Policies > Product Policies > Batch > Equipment Editor > Access Modes.
- Right-clickAccess Modes, and then selectProperties. TheAccess ModesPropertiesdialog box opens.
- In theFull Editrow, select theConfigure Securitybrowse button. TheConfigure Securable Actiondialog box opens.
- SelectAdd. TheSelect User and Computerdialog box opens.
- In theFilter Usersbox, selectShow All.
- InUsers, selectENG.
- SelectOK. TheConfigure Securable Actiondialog box is updated, showing ENG in the list ofUserswith theAllowcheckbox selected.
- SelectOKto close theConfigure Securable Actiondialog box.
- In theAccess Modes Propertiesdialog box, selectView Only.
- In theView Onlyrow, select theConfigure Securitybrowse button. TheConfigure Securable Actiondialog box opens.
- SelectAdd. TheSelect User and Computerdialog box opens.
- In theFilter Usersbox, selectShow All.
- InUsers, selectOPER.
- SelectOK. TheConfigure Securable Actiondialog box is updated, showing OPER in the list ofUserswith theAllowcheckbox selected.
- SelectOKto close theConfigure Securable Actiondialog box.
- SelectOKto close theAccess Modes Propertiesdialog box.
See the for more information on security.
FactoryTalk Batch
Administrator GuideProvide Feedback