Rebuild the recipe directory
The working set of recipes is stored in the location specified on the
Project
Settings
tab of the FactoryTalk Batch Equipment Editor
Server Options
dialog box. If a recipe has been added to or deleted from this recipe
storage location without using the FactoryTalk Batch Recipe Editor
, rebuild the recipe directory.- There are two options:
- If theFactoryTalk Batch Recipe Editoris closed, open it to rebuild the recipe directory. Any recipe file additions or deletions are shown when using theOpen, Remove, Import, Export, orGenerate Reportsmenus in theFactoryTalk Batch Recipe Editor.
- If theFactoryTalk Batch Recipe Editoris already open, selectFile > Rebuild Recipe Directory. TheFactoryTalk Batch Recipe Editorreads all of the currently stored recipes and updates the recipe directory file.
- If a recipe version conflict occurs when rebuilding the directory, theResolve Version Conflict for Rebuild Recipe Directory Requestdialog box opens. A prompt opens to retain one of the two recipes that conflict.TIP:If there are unverified recipes in the recipe directory, the option to verify all recipes or verify and validate all recipes displays.
Provide Feedback