The eProcedure Server
e
Procedure ServerFor ease of understanding, and for tutorial purposes, this guide refers to configuring and
using the sample files installed with
FactoryTalk
Batch. The SampleDemo folders contain complete area models and recipes for a simulated
plant. Before running the demonstrations, you must add a FactoryTalk
Security user, configure the FactoryTalk Batch
Server to recognize the required project directories, select the initialization path and
file name, and then start the FactoryTalk Batch
Server, the FactoryTalk
eProcedure
Server, and the FactoryTalk Batch
Phase Simulator.
TIP:
This guide outlines the configuration and use of the
SampleDemo demonstration files. It is recommended that you follow the directions for using
this demonstration step by step.
The
FactoryTalk
eProcedure
Server provides the services to the FactoryTalk Batch
Server to enable the use of HTML instruction files. Communication from FactoryTalk Batch View
to the eProcedure
Server uses HTTPS. FactoryTalk
eProcedure
uses OLE for Process Control (OPC) for communications between the eProcedure
Server and the FactoryTalk Batch
Server.The
eProcedure
Server coordinates the following functions:- Provides the services to theFactoryTalk BatchServer to enable the use of HTML instruction files.
- Formats parameters and report parameters from material-based recipes into instruction files.
This section assumes that the for more information.)
FactoryTalk
eProcedure
Server, the FactoryTalk Batch
Server, and FactoryTalk Batch View
have been installed and configured. (See the FactoryTalk Batch
Components Upgrade and Installation GuideProvide Feedback