Start FactoryTalk Batch Phase Simulator

FactoryTalk Batch
comes with a phase logic simulation program, referred to as the
FactoryTalk Batch
Phase Simulator used to simulate the batch process without connecting to a PCD. The Phase Simulator imitates the functionality of a data server and can communicate with the
FactoryTalk Batch
Server using OPC communication protocol. The Phase Simulator is a powerful tool for testing, experimentation and demonstration purposes. In this guide, run the sample demonstration using the Phase Simulator.
TIP:
If the Phase Simulator is required and OPC protocol is used for communications, the
FactoryTalk Batch
Server automatically starts the Phase Simulator. Check the Windows taskbar to see if the Phase Simulator is started.
To run the sample demonstration correctly, open the
ice_cream1.sim
file in the Phase Simulator.
To start
FactoryTalk Batch
Phase Simulator:
  1. If the Phase Simulator is already running, maximize it from the Windows taskbar. If the Phase Simulator is not running, select
    Start > Rockwell Software >
    Simulator
    . The
    FactoryTalk Batch
    Phase Simulator opens.
  2. IMPORTANT:
    Administrator privileges are required to perform this procedure.
    Select
    File
    >
    Open
    . The
    Open Simulator Configuration File
    dialog box opens.
  3. From the
    Look in
    list, open the
    Program Files > Rockwell Software > Batch > SampleDemo1 > Recipes
    folder. Select the
    ice_cream1.sim
    file, and then select
    Open
    .
  4. Minimize the
    FactoryTalk Batch
    Phase Simulator
    window.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal