Use ACM Tools
Use
Application Code Manager
tools to assist in reusable code development and management.This table describes each of the tools.
Tool | Description |
|---|---|
Use to import or export ACM project content between Excel spreadsheets (Schedule). Use for bulk additions, duplications, changes; comparing versions; snapshots; backup customer parameter entry, and/or transferring project contents. | |
Use to create, delete, upgrade, back up, and restore ACM databases. | |
Plugins | Add capabilities to Application Code Manager by installing plugins through the
TOOLS > Plugins command. |
Log Debug Information | Choose to include debug information in the ACM Log File to help with troubleshooting applications. Information is written to the ACM log file when design outputs are generated, (for example, <CLX>, FactoryTalk View , FactoryTalk Historian , and Word) or when schedules are imported or exported. |
Log Viewer | Use to view the contents of the most recent ACM log file. An ACM log file is
created for each ACM session. |
Settings | Use to set the location of the system documentation, the language, and the
default settings for ControlLogix® controllers. |
Document Template Editor | Use to develop and test document generation templates. |
Open Target ACD | Opens the directory and allows navigation to the ACD file location. Use to instantiate library content into an existing file, versus creating an ACD
file. |
Find Compatible Logix Designer Version | Use to check the availability of a compatible Studio 5000 Logix Designer
version. |
Provide Feedback