Document Template Editor
How do I open the Document Template Editor?
- From theTOOLSmenu, selectDocument Template Editor.
The
Document Template Editor
provides an environment to develop and test document generation templates.
TIP:
The ability to use this is only available if the product has a Standard activation license and is not available in Lite mode.
The
Document Template Editor
includes the following functions:- Highlights reserved words in the template language.
- Folds repeat blocks.
- Error checking and highlighting.
- Ability to save frequently used code fragments for later reuse.
- Generates an output template file.
Provide Feedback