Log File Viewer
The Log File Viewer provides a quick way to view the most recent events sent to the ACM log file. The Log File Viewer can be opened from the
TOOLS
menu of Application Code Manager
and from the TOOLS
menu of Import Export Manager.The Log File Viewer displays errors, warning, informational, and debug events in a grid.
At the top of the Log File Viewer, a set of buttons list the types of log entries and the number of entries for each type:

The entries displayed in the event grid can be filtered by type of events by clicking the button corresponding to the item to remove from the list.
When an item is not included in the view, the button is shaded gray:

By default, Log File Viewer displays events in ascending date time order.
The order can be changed to be either ascending or descending and be based on any of the columns displayed in the events grid. Click the column heading to sort the display by
Type
, Date/Time
, or Description
. A small arrow appears next to the column heading being sorted and denotes whether the current sort order is by ascending (up arrow) or descending (down arrow) values.Provide Feedback