Log Debug Information
To assist in troubleshooting
Application Code Manager
, enable logging of debug information to the ACM Log File.Information is written to the ACM log file when design outputs are generated, (for example, <CLX>,
FactoryTalk View
, FactoryTalk Historian
, and Word) or when schedules are imported or exported.Once the additional logging information is no longer needed, disable log debug information.
To log debug information
- ClickTOOLS > Log Debug Information.A check mark appears next to theLog Debug Informationentry in theTOOLSmenu. Clicking the item again disables logging of debug information.
Provide Feedback